Lenel (F) Integration Note

2.2.png

FLIR Latitude VMS - Fenel (F) Integration

Background

The FLIR - Lenel (F) module integrates the FLIR Latitude VMS with Lenel’s OnGuard access control system. The integration provides the means for handling targeted access control events generated by OnGuard within Latitude. Users can create an OnGuard server representation in Latitude and view OnGuard panels, readers, alarm inputs/outputs from within Latitude’s tree and maps modules. OnGuard access control and system events can both be monitored in Latitude and configured to trigger an alarm or dispatch an event. Using Latitude’s Events / Actions infrastructure, users can further configure Latitude actions to be executed upon access control alarms or events.

 

Key Features

  • Represent OnGuard panels and readers in the VMS trees and maps
  • Drag and drop readers to Control Center tiles to display video from their associated cameras
  • Perform access control operations, such as opening doors, from the VMS trees and maps
  • Trigger VMS alarms and events upon incoming access control events
  • Configure additional VMS actions to be executed upon incoming access control events
  • Query for recorded video by access control originating information
  • Control Center displays full description of the access control event: Event name, time of event, name and ID of the reader, etc. If the event is related to a specific person, the name of the person and the card ID are displayed as well.
  • OnGuard entity icons in Latitude trees and maps reflect their accessibility statuses

2.3.png

 

Specifications

2.4.PNG

*ACS = Access Control System

 

Ordering Information

2.5.PNG

 

Prices

Prices shall be according to FLIR’s then-current dealer price list applicable to Company’s Territory (Dealer Prices). FLIR may change Dealer Prices at any time (Price Change). Price Changes shall be effective thirty (30) days after FLIR issues notice of the Price Change to Dealer. Price Change shall apply to Orders accepted after the effective date of a Price Change.

Back to top