Reduce energy costs by ending hidden leaks

Today's soaring energy costs can have a huge impact on a company's bottom line, especially for manufacturers who rely on compressed air and vacuum systems or use gases such as carbon dioxide in their production process. When these systems leak—it's like money seeps out along with the air. So being able to see the system leaks, pinpoint the source, and even calculate the energy loss with a detection system is a game changer. 

The FLIR Si-Series are acoustic imaging cameras for leak detection: your perfect solution for locating pressurized leaks in compressed air systems, faults in vacuum systems, and CO2 leaks. Whether you choose the Si2-Pro, Si2-LD, Si124-LD Plus, or any Si-Series camera, our lightweight, one-handed cameras can help you identify efficiency loss and potential failures up to 10 times faster than traditional methods, and with minimal training.

See How it Works

Find leaks and analyze energy savings

FLIR Si2-LD and Si2-Pro

Through a regular maintenance routine, the FLIR Si-Series can help facilities save money on utility bills and delay the expense of installing new compressors.
View Product

 

How Acoustic Leak Detection With the FLIR Si2-Series Can Benefit Your Industry

Why Acoustic Imaging Detection?

Compressed air may be cheap but the power needed to run faulty systems is not. By catching leaks through detection systems and sensors early, facilities crews have the opportunity to prevent further energy waste and can schedule repairs rather than risk shutting down operations to replace an entire system.

It's a proactive stance against leaks

Leak detection with an acoustic imager leads to improved energy efficiency and reduced costs, not only from repairs to compressed air and vacuum systems but also related to any expensive specialty gases that could be leaking during your production process. FLIR Si-Series acoustic imagers can calculate your energy savings while you're still in the field, so you can instantly see how soon you'll get a return on your investment

FLIR Si-Series acoustic imaging cameras use machine learning to distinguish the other characteristics of the sound pattern created by leaks from the background. It is the same way you distinguish between a harmonica and a bell playing the same note. Combining that with the ability to actually see the leak on a screen allows technicians to pinpoint leak locations almost instantly.

It's a proactive stance against leaks

 

 

 

Request Info

Optin

By submitting you agree to FLIR's privacy policy and cookie policy.

Related Content

Application Story

Capturing Hidden Air Leaks in Time Prevents Serious Incidents and Saves Costs at a Pharmaceutical Plant

Read More
Application Story

Detecting Faults in High Pressure Hydraulic Systems with Acoustic Imaging Cameras

Read More
Application Story

Discovering Hidden Air Leaks in Time Improves Productivity and Competitiveness in the Automotive Industry

Read More
Whitepaper

How Manufacturing Facilities Speed Up Inspection with Acoustic Imaging

Read More
Case Study

Leak Detection in Compressed Air Systems: A Case Study of Air Power East's Success with the FLIR Si124 Acoustic Imaging Camera

Read More
Application Story

Reducing Carbon Dioxide Emissions With an Acoustic Air Leak Detector

Read More
Application Story

Silent Leaks, Resounding Savings: How Acoustic Imaging Is Saving Pennine Healthcare Thousands

Read More
Fundamentals

Detecting Air Leaks and Mechanical Faults in ATEX Zone 22 with the FLIR Si2x Acoustic Imaging Camera

Read More