For example, could I have 4 images of the same component taken over a year all on the same page. Then beneath that could I use the trend tool to trend its temperatures? Would I be able to create a report with this layout on each page through multiple pages?
In Reporter 8.1 and 8.2 you can place one trend graph on each page and connect it to the images on the same page. The Wizard does not have an automatic way to connect the trend graph to other images than defined in the template so there will be some manual work in the finished report. This is however an easy task and the final report will have the shape you look for. Please find attached an example showing increasing temperature of a heat source.
File Attachment(s)
- File Type PDFDocument1.PDF (70.97 KB)