186 frames is the size of the burst memory.Time of recording depends on how you set recording condition. Maximum frame rate is 30Hz. From this you can set to skip 2-255 frames between savings, allowing down to 0.12Hz
For longer sequences, you will need firewire connection to a PC with ThermaCAM Researcher or an application built with our SDK.