In order to make it work, you have to make sure the following sofware and drivers versions are installed.
- ResearchIR 4.40.4.17 or later, downloadable from CustHelp;
- Active Silicon runtime version 1.3.1 (ONLY)
- AS driver 1.7.0.0 (ONLY), included in the CXP Firebird installer package 1.3.1 below; - see download page
-
- 32bit version
- 64bit version
IMPORTANT:
With camera set in single link mode, do not wire both coax connectors and connect only link 0 (on the camera).