I would like to know if a Pro Template may contain more than one inspection page.

In case the answer is yes, how to select the desired page in the wizard? Application : I am an operator doing inspections on power lines. There exist 4 different voltages. Each voltage has his own inspection page. Can I create a single report, from the same template, with (for instance) 3 inspection pages related to 400 kV, 3 related with 225 kV, and one with 90 kV. This was possible with ThermaCAM Reporter 2000.

Yes, the template can contain more than one "IR page type". First, select the template page you want for the first set of IR images and add those. Then go back and select another page from the template and continue adding IR pages. And so on. Attached is one simple example using the "View IR" template.

Back to top