Is it possible to change the object parameters in the Flir K series cameras?

Object parameters in the FLIR K series are set to the following and are not possible to change.

  • Emissivity: 0.95
  • Atmospheric temperature: +60°C (+140.0°F)
  • Relative humidity: 75%
  • Distance to object: 3.0 m (9.8 ft.)

Object parameters are used in the formula to calculate the object temperature.

Back to top