Is it possible to see the thermal changes in a hand warmer with a thermal camera?

This is a video of the crystallisation process taking place in a hand warmer. The process is recorded with ResearchIR and the camera is a FLIR A655SC camera. The color scale is linearly locked to the span (23–65°C), and no histogram equalization or image enhancements were used.

Back to top