Streaming video via USB is not possible on a Vista system because we use a network server in the camera to distribute video. At the moment we don't have a network driver signed by Microsoft which is required to comply with the security system of Vista.
FLIR IR Camera Player 2.1.1 and 2.1.2 work on Vista 32-bit.
FLIR IR Camera Player 2.1.2 works on Vista 64-bit
All our present analysis programmes (Reporter 8.3, QuickReport 1.2, Researcher 2.9) are fully verified to run on Vista systems. Images that are saved in the camera are easily copied to the PC for analysis if you set the USB port of the camera as "Mass storage device"