The position calculated by a GPS receiver requires the current time, the position of the satellite and the measured delay of the received signal. The position accuracy is primarily dependent on the satellite position and signal delay.
GPS horizontal position fixes are typically accurate better then 15 meters (50 ft).
The GPS transmitting protocol is : WGS 84