What is the typical spectral response for certain camera/lens combination?

  

This curve is valid for the following lenses:
  • IR lens, f=88.9 mm (7°)
  • IR lens, f=41.3 mm (15°)
  • IR lens, f=24.6 mm (25°)
  • IR lens, f=13.1 mm (45°)

 

This curve is valid for the following lenses:
  • IR lens, f=6.5 mm (80°)
  • Close-up IR lens, 2.9× (50 µm)
  • Close-up IR lens, 5.8× (100 µm)

 

This curve is valid for the following lens:
  • Close-up IR lens, 1.5× (25 µm)
Back to top