The battery is a rechargeable Li-Ion battery (3.6 V, 4.4 Ah) and the camera will run > 4 hours with a fully charged battery when the battery is new.
The battery will fully charge in 4 hours.
The life expectancy is > 300 charging cycles (> 70% of minimum capacity).
Approximate lithium content is 1.32 g
Below is the specification for the battery status indicator:
The in-truck charger is an accessory that can be used to charge the camera and/or a spare battery. The charger is a smart charger and will not overcharge the batteries.
The charging status is indicatde by the LED indicator.
- Indicator LED blinking: Battery is charging.
- Indicator LED constant light: Battery is fully charged.
- Indicator LED off: No device attached.