Why can't I install the eBUS drivers in ResearchIR/QuickPlot ?

eBUS installation on Windows XP

If the user connects to a A325 camera and has not the eBUS driver from Pleora a warning will appear in the log.

Driver warning message

When clicking on the blue link the following dialog will appear:

 
Before pressing OK it is important to uncheck the "Protect my computer…" checkbox in order to have a successful installation.

After this the eBUS installation tool will launch and the eBUS universal driver can be installed

 

Back to top