How can I update my FLIR camera firmware?

Modern FLIR handheld cameras such as the C, E, and K series can easily be updated using the FLIR Tools PC software. Note that your camera needs to be registered first.

To update the camera:

1. Power up the camera, connect it to the PC with a USB cable, and then start FLIR Tools.  If your camera uses an SD card, ensure that the card is inserted into the camera.

2. If the splash screen appears, click Check for Updates.  For the K-series firefighting cameras, click Configure Camera, then Check for Updates.

3. You can also click Check for Updates from the Help menu in FLIR Tools.

 

4. If an update is found, it will show the new version and, if it is registered, you can proceed with the update.

Related Articles