Teledyne FLIR Pan-Tilt Web Control
![](/globalassets/industrial/oem/ptu/ptu-web-control.jpg)
The PTU contains a Web-based interface that allows you to test and program various functions. This interface is accessible via the Ethernet connection on the breakout cable.
- To connect, power on, and test the PTU using the Ethernet connection and Web interface:
-
Connect one end of an RJ-45 Ethernet cable to the PTU-E46 controller, and then connect the other end of the cable to the host computer, either directly or through a router/hub.
-
Connect a power source to the PTU, making sure to incorporate a readily accessible power disconnect (such as a power strip) to allow safe power removal from the system.
-
Ensure that the PTU is clear to move in both axes (pan and tilt) without hitting any obstructions before applying power.
-
Power on the PTU. By default, the PTU will begin a calibration sequence that will cause it to move from its current position to the center (0) positions in both axes.
-
Launch a Web browser. The PTU supports modern versions of the Microsoft Internet Explorer®, Mozilla® Firefox®, and Google® Chrome® browsers with JavaScript enabled.
-
Run the PTU Finder utility from the CD included with your PTU package. A list of the individual PTUs currently connected to the network and their corresponding IP addresses will appear in the application window.
-
In your browser, navigate to the appropriate IP address (such as http://192.168.1.101). A web page appears when you are connected to the selected PTU.
- The PTU Web interface allows you to configure the network interface, configure various parameters, and control the PTU.
- Navigate to the PTU Control page.
11. Click the arrows to pan and tilt the PTU and verify that it is working properly.
Please refer to the Pan-Tilt E Series Command Reference Manual for instructions on using the Web interface.
Reference: PTU Configuration Web Page